System Backup
| Description |
Use one of the USB ports inside the Control Box (CB) when doing a Backup and Restore operation. Using a CB USB port is more stable and running a Backup requires less time.
If you restore a system with a new SD card, you must match the Serial Number in the new SD card image when you start up Polyscope.
Failure to match the Serial Number can result in an incomplete restore process. A restore error appears for not finding the matching serial number
|