You can set up the safety limits for each set of safety parameters, creating distinct configurations for normal, or higher settings, and reduced.
The reduced configuration is active when the tool/end effector is positioned on the reduced side of a Trigger Reduced Plane, or when the reduced configuration is externally triggered by a safety input.
Using a plane to trigger the Reduced configuration: When the robot arm moves from the side of the trigger plane configured with reduced safety parameters,
to the side that is configured with normal safety parameters, there is a 20 mm area around the trigger plane where both normal and reduced limits are allowed.
This area around the trigger plane prevents nuisance safety stops when the robot is exactly at the limit.
Using an input to trigger the Reduced configuration: When a safety input starts, or stops, the reduced configuration, up to 500 ms can elapse before the new
limit values become active. This can happen in either of the following circumstances:
The robot arm adapts to the new safety limits within the 500 ms.
|