Safety Message Types

Safety messages and statements are used throughout this manual to emphasize important information.
Read all messages and statements to help ensure safety and to prevent injury to personnel and product damage.

The safety message types are defined below.

Indicates a hazardous situation which, if not avoided, could result in death or serious injury.
Indicates a hazardous electrical situation which, if not avoided, could result in death or serious injury.
Indicates a hazardous hot surface where injury can result from contact and non-contact proximity.
Indicates a hazardous situation which, if not avoided, could result in injury.
Indicates grounding.
Indicates protective grounding.
Indicates the risk damage to equipment and/or useful information that should be particularly noted.
Indicates more detailed information that should be consulted in the manual.

This warning draws attention to procedures which serve to prevent or remedy emergencies or malfunctions:

Procedures marked with this warning must be followed exactly.