Accessing Linux Partition from Windows

With the software from Paragon you can access all partitions on the SD-card.

The files needed are located on the partition called: datafs

If the partition is not shown, it could be due to the files not being mounted automatically.

To correct this:

  1. Open the Paragon software.

  2. Select the partition (1).

  3. Select the Mount icon (2).

  4. Select the Volume drive letter (3).

  5. Then Mount (4).