Adding External Equipment for Troubleshooting Purpose

For troubleshooting it can be useful to add a mouse, keyboard or monitor.
Most USB mouse and keyboards are supported. Plug in the mouse or keyboard in one of the available USB ports. It may be required to restart the Control Box for it to work.

In the Control Box, a Mini Display Port is available. When a monitor is connected, it will display the same contend as the Teach Pendant and can be connected at the same time as the Tech Pendant. It may be required to restart the Control Box for it to work.