How to Access Linux Partition from Windows
With the software from Paragon you can access all partitions on the SD-card.
The files needed are located on the partition called datafs
If the partition is not shown, it could be it is not mounted automatically.
To correct this, open the Paragon software, select the partition (1), select the Mount icon (2), select the Volume drive letter (3) then Mount (4).