Downgrading vs. Restoring system backup
Do not downgrade the robot software to an earlier version than the version the robot was manufactured.
Do not revert your robot software using older update packages if you have software version equal or above 5.8 installed. If for any reason, you need to downgrade below PolyScope version 5.8, you can do so by restoring your old system backup (system backup was implemented from Polyscope version 5.5 ahead).
The system backup requires around 4Gb memory, please use a USB stick of 4Gb or more capacity.
Always perform program and installation files backup before updating the software.