Export From Robot Tab

The Export from Robot tab allows you to create and export the Support File from your connected robot via ethernet connection to the computer. Refer to 2.5.5 Record Data tab topic in this manual, to understand how to connect the robot’s and computer IP addresses.

For older robot software versions (PolyScope 5.7 and 3.12 below) the Log History and Flight Reports are retrieved instead of the Support File.

After the download the user will be asked, if he/she wants to open the pulled data directly on UR Log Viewer or just store in the computer.