Your Product
| Product |
The Base-mounted Range Extender 40m, for UR3e and UR5e is an accessory used to extend the cable length between robot and controller. It includes a 40-meter cable (power and communication) and active signal repeaters - one at the robot end and the other at the controller end - for reliable performance over long distances. It is designed for OEM controllers with UR3e and UR5e robots in Welding applications where longer separation between robot and controller is required.
The Base-Mounted Range Extender consists of the following components:
This manual describes all of the components. This manual should also be used, if you have purchased any one part as a single component.
|