Remote ON/OFF Control and Emergency Stop
The OEM Control Box requires a remote ON/OFF control and an emergency stop push-button. The following sections describe how to install them using the I/O ports.
Connecting the ON/OFF control
The images below show how the remote ON/OFF control is connection.
1 | Status: On | 2 | Status: Off |
Connecting the Remote Emergency Stop
Install an external Emergency Stop (E-stop) if the Teach Pendant with the default Emergency Stop is not connected to the Control Box.
The following illustration shows the minimum required Emergency Stop installation.