Quick System Start
|
Before using the PolyScope , verify the robot arm and Control Box are correctly installed.
This is how you quickly start up the robot.
-
On the Teach Pendant, press the emergency stop button.
-
On the Teach Pendant, press the power button and allow the system to start, displaying text on the PolyScope.
-
A popup appears on the touch screen indicating that the system is ready and that the robot must be initialized.
-
In the popup dialog, tap Go to Initialize Screen to access the Initialize screen.
-
Unlock the emergency stop button to change robot state from Emergency Stopped to Power off.
-
Step outside the reach (workspace) of the robot.
-
On the Initialize Robot screen, tap the ON button and allow robot state to change to Idle.
-
In the Payload field, in Active Payload, verify the payload mass. You can also verify the mounting position is correct, in the Robot field.
-
Tap the Start button, for the robot to release its brake system. The robot vibrates and makes clicking sounds indicating it is ready to be programmed.
|