Robot Cable

Replacing Robot Cable

The maximum robot connection from the robot arm to the Control Box is 12 m. Improper robot connection can result in loss of power to the robot arm.
  • Do not extend beyond 12 m.
  • Do not make the connection from robot to control box shorter than 6 m.
Connecting the Base Flange Cable directly to any Control Box can result in equipments or property damage.
  • Do not connect the Base Flange Cable directly to the Control Box.
  1. On the base of the robot arm, locate the robot connection and twist it to the Open position.
  2. Pull the robot connection apart to separate the Robot Cable from the Base Flange Cable.
  3. On the Control Box, locate the robot connection cable and twist it to the Open position.
  4. Pull the robot connection apart to separate the Robot Cable from the Control Box connector.
  5. Connect the new Robot Cable to the Base Flange connector and twist to the Closed position.
  6. Connect the new Robot Cable to the Control Box connector and twist to the Closed position