Assembling Clamp Connection
The assembly is done in reverse of the disassembly. However, a few things must be noted before assembly is begun.
Replace the foam seal on the clamps if damaged to maintain the IP classification.
Replace the wear rings if extensive wear or damage is shown.
The dots must be aligned otherwise the connection cannot be made.
|
|
|
![]() |
|
|
Ensure the screws are inserted in the correct clamp.
Only apply to early version of brackets where one side has a circular marker.
When tightening the clamps, it must be done in steps. Do not exceed recommended torque:
- Step 1: Tighten one side so there is a gap of 1.0mm to 1.5mm.
- Step 2: Tighten the other side completely with 4.0Nm. +/- 0.50 Nm.
- Step 3: Tighten the first side with 4.0Nm. +/- 0.50 Nm.
- Step 4: Ensure same gap at both ends.
|
|