pow(base, exponent)
Returns base raised to the power of exponent
Returns the result of raising base to the power of exponent. If base is negative and exponent is not an integral value, or if base is zero and exponent is negative, a runtime error is raised.
Parameters
base:
floating point value
exponent:
floating point value
Return Value
base raised to the power of exponent
Example command: pow(5.,3)
- Example Parameters:
- Base = 5
- Exponent = 3
- Returns 125.