Single Step in a Program
| Description |
Single Step allows the current program to be exectued one node at a time, when the robot is in Manual mode. (See Operational mode).
This is useful when you are checking your program for errors.
|
|
Single Step |
Single Step allows the selected program node to run, then pauses at the beginning of a new node. Single Step can only be used when the current program is paused. If you want to use Single Step on a specific node, the node must also support Breakpoints.
|