Backdrive
Description |
Backdrive is a Manual Mode used to force specific joints to a desired position without releasing all brakes in the robot arm. This is sometimes necessary if the robot arm is close to collision and the vibrations that accompany a full restart are not desired. The robot joints feel heavy to move, while Backdrive is in use.
You can use any of the following sequences to enable Backdrive:
|
3PE Teach Pendant |
To use the 3PE TP button to backdrive the robot arm.
|
3PE device/switch |
To use a 3PE device/switch to backdrive the robot arm.
|
Freedrive on robot |
To use Freedrive on robot to backdrive the robot arm.
|