Digital Output Mode
| Description |
The tool communication interface allows two digital outputs to be independently configured. In PolyScope, each pin has a drop-down menu that allows the output mode to be set. The following options are available:
After selecting a new output configuration, the changes take effect. The currently loaded installation is modified to reflect the new configuration. After verifying the tool outputs are working as intended, make sure to save the installation to prevent losing changes.
|
| Dual Pin Power |
Dual Pin Power is used as a source of power for the tool. Enabling Dual Pin Power disables default tool digital outputs.
|