| Conveyor Parameters
|
- Incremental Encoders
- These can be connected to Digital Inputs 8 to 11. Decoding of digital signals runs at 40kHz. Using a Quadrature encoder (requiring two inputs), the robot can determine the speed and direction of the conveyor. If the direction of the conveyor is constant, a single input can be used to detect Rising, Falling, or Rise and Fall edges which determine conveyor speed.
- Absolute Encoders
- These can be connected through a MODBUS signal. This requires a Digital MODBUS Output register preconfigured in (section ).
-
|