Expression Editor

Description

The expression editor has a number of buttons and functions for inserting the special expression symbols, such as * for multiplication and for less than or equal to. Expressions are edited as text.

All defined variables can be found in the Variable selector, while the names of the input and output ports can be found in the Input and Output selectors. Some special functions are found in Function.

 

Expressions in Editor

When your expression is complete, you can tap the Submit button to check for grammatical errors. The Esc button exits the screen and discards all unsaved changes.

 

Example

digital_in[1]

True and analog_in[0]<0.5