Using Selected Program Nodes
Description |
You can start your robot program from any program node in the program tree. This is useful when you are testing your program.
When the robot is in Manual Mode (see Operational mode), you can allow a program to start from a selected node or you can start the entire program from the beginning.
|