tool_wrench_limit_set(frame_offset, Fx, Fy, Fz, Mx, My, Mz)
Limit the wrench (forces and torques) caused by motion of the robot in a frame given relative to the tool flange. The wrench is limited in normal and reduced mode operation, as well as during protective stops, safeguard stops, 3PE stops and emergency stops. For this reason, it can affect robot motion speed to ensure adherence to safety limits. Usage can help prevent dropping items by limiting accelerations as well as reducing wrench applied to the attached tool.
This limitation does not affect the forces and torques that can be applied in force control.
Parameters:
frame_offset: Pose specifying frame relative to the tool flange similarly to how the TCP offset is specified. The first three coordinates specify translational offset along the x- y- and z-axis in meters. The last three specify the rotational offset using the axis-angle representation in radians.
Fx (optional): Float, setting maximum acceleration force along the X-axis in the specified frame.
Fy (optional): Float, setting maximum acceleration force along the Y-axis in the specified frame.
Fz (optional): Float, setting maximum acceleration force along the Z-axis in the specified frame.
Mx (optional): Float, setting maximum acceleration torque around the X-axis in the specified frame.
My (optional): Float, setting maximum acceleration torque around the Y-axis in the specified frame.
Mz (optional): Float, setting maximum acceleration torque around the Z-axis in the specified frame.
Any optional parameter not specified means the axis is only limited by standard robot limitations.
Example command: tool_wrench_limit_set(p[0, 0, 0.1, 0, 0, 1.57], Mx=10, My=15)
Example Parameters:
-
frame_offset = p[0, 0, 0.1, 0, 0, 1.57] → limitation will be applied in a frame offset 10 cm in front of the tool flange rotated by 45 degrees around the axis of displacement.
-
Mx = 10 → acceleration torque will be limited to 10 Nm around the X-axis in the specified frame.
-
My = 15 → acceleration torque will be limited to 15 Nm around the Y-axis in the specified frame.
Remaining forces and torques will not be limited by this algorithm.
Example command: tool_wrench_limit_set(get_tcp_offset(), Fz=50)
Example Parameters:
-
frame_offset is equal to the active TCP offset.
-
Fz = 50 → acceleration force is limited such that force does not exceed 50 N along the Z-axis in the TCP frame.
The set limit is persisted until shutdown of the controller or until explicitly disabled by executing tool_wrench_limit_disable().