set_tool_voltage(voltage)

Sets the voltage level for the power supply that delivers power to the connector plug in the tool flange of the robot. The votage can be 0, 12 or 24 volts.

Parameters

voltage: The voltage (as an integer) at the tool connector, integer: 0, 12 or 24.

Example command: set_tool_voltage(24)

  • Example Parameters:
    • voltage = 24 volts