read_input_boolean_register(address)
Reads the boolean from one of the input registers, which can also be accessed by a Field bus. Note, uses it’s own memory space.
Parameters
address:
Address of the register (0:127)
Return Value
The boolean value held by the register (True, False)
Note: The lower range of the boolean input registers [0:63] is reserved for FieldBus/PLC interface usage. The upper range [64:127] cannot be accessed by FieldBus/PLC interfaces, since it is reserved for external RTDE clients.
>>> bool_val = read_input_boolean_register(3)
Example command: read_input_boolean_register(3)
- Example Parameters:
- Address = input boolean register 3