normalize(v)
Returns the normalized form of a list of floats
Except for the case of all zeroes, the normalized form corresponds to the unit vector in the direction of v.
Throws an exception if the sum of all squared elements is zero.
Parameters
v: List of floats
Return Value
normalized form of v
Example command:
normalize([1, 0, 0])-> Returns [1, 0, 0]normalize([0, 5, 0])-> Returns [0, 1, 0]normalize([0, 1, 1])-> Returns [0, 0.707, 0.707]