interpolate_pose(p_from, p_to, alpha)
Linear interpolation of tool position and orientation.
When alpha is 0, returns p_from. When alpha is 1, returns p_to. As alpha goes from 0 to 1, returns a pose going in a straight line (and geodetic orientation change) from p_from to p_to. If alpha is less than 0, returns a point before p_from on the line. If alpha is greater than 1, returns a pose after p_to on the line.
Parameters
p_from: tool pose (pose)
p_to: tool pose (pose)
alpha: Floating point number
Return Value
interpolated pose (pose)
Example command: interpolate_pose(p[.2,.2,.4,0,0,0], p[.2,.2,.6,0,0,0], .5)
- Example Parameters:
- p_from = p[.2,.2,.4,0,0,0]
- p_to = p[.2,.2,.6,0,0,0]
- alpha = .5
- Returns p[.2,.2,.5,0,0,0]