get_inverse_kin_has_solution(pose, qnear, maxPositionError=1E-10, maxOrientationError=1e-10, tcp="active_tcp")
Check if get_inverse_kin
has a solution and return boolean (True) or (False).
This can be used to avoid the runtime exception of get_inverse_kin
when no solution exists.
Parameters
pose:
tool pose
qnear:
list of joint positions (Optional)
maxPositionError:
the maximum allowed position error (Optional)
maxOrientationError:
the maximum allowed orientation error (Optional)
tcp:
tcp offset pose (Optional)
Return Value
True if get_inverse_kin
has a solution, False otherwise (bool)