Introduction
The Universal Robot can be controlled at two levels:
-
The PolyScope or the Graphical User Interface Level
-
Script Level
At the Script Level, the URScript is the programming language that controls the robot.
The URScript includes variables, types, and the flow control statements. There are also built-in variables and functions that monitor and control I/O and robot movements.