Connecting the USB-to-Ethernet adapter
Criteria for success
-
The USB-to-Ethernet adapter is connected to the LAN cable and the Control Box USB port.
Before you connect the USB-to-Ethernet adapter
-
Locate the USB port in your Control Box before inserting the USB-to-Ethernet adapter.
-
Use a USB hub if the Control Box USB panel port is occupied.
To connect the USB-Ethernet adapter
-
Connect the LAN cable to the Ethernet port in the USB-to-Ethernet adapter.
-
Connect the USB-to-Ethernet adapter to the USB port in the Control Box.
| 1 | USB port | 2 | USB-to-Ethernet adapter |
| 3 | Locknut | 4 | LAN Cable |
Figure 80.6: USB-to-Ethernet adapter connected to LAN cable locked into cable gland.
In the next section you are going to pair and install the URCap.