Installing the URCap
This procedure has the following success criteria:
-
Install software (the URCap) on the robot that connects to the cloud solution, using the provided USB flash drive.
Using myUR Monitoring with a corrupted USB flash drive can result in corrupted files, and/or viruses being downloaded to the robot.
-
Always use the provided USB flash drive.
To install the myUR Monitoring URCap:
-
In the PolyScope Header, tap the Hamburger menu and access Settings > System > URCaps.
-
Tap the + button to select URCap.
-
Navigate to the desired file in the list and tap to open it.
-
Tap Restart. If correctly installed, the new URCap appears under Active URCaps.
-
Navigate to Installation > URCaps > myUR.
-
Tap Install to install cloud communication software.
-
For CB3 robots: reboot the robot, to establish connection.