Icons

Header Icon

Icon Title Description

Program name

Gives access to System Manager.

Enables you to create, modify, add program, and URCaps files.

Left Toolbar Icons

Icon Title Description

More

Access to information of robot version, serial number, and settings.

Application

Configures and sets up the robot arm settings and safety, including end effectors and communication.

Program

Access to basic and advanced robot programs.

3D

Enables control and regulation of robot movement in X, Y, Z coordinates.

Operator

Operates the robot using prewritten programs and shows the status of the robot.

Icons Inside the More/Hamburger Icon

Icon Title Description

System Manager

Gives access to System Manager.

Enables you to create, modify, add program, and URCaps files.

About

Displays information about robot version and serial number.

Settings

Configures system settings, such as language, units, password, and security.

Reload

A safe function to apply the default settings defined in the application.

Shutdown

To restart, power on and off the robot.

Right Toolbar Icons

Icon Title Description

Safety Overview

Access to the active safety checksum and detailed parameters of each robot arm parts, and changes the operational mode.

Move

Comprehensive function for robot movement, detailing the joints, TCP, flange, base.

Program structure

Provides an orderly structure of created program(s). Access to add modules.

Global Variables

Access to created program names and values.

Footer Icons/Buttons

Icon Title Description

Initialize

Manages the robot state. When RED, press it to make the robot operational.

  • Black, Power off. The robot arm is in a stopped state.

  • Orange, Idle. The robot arm is on, but not ready for normal operation.

  • Orange, Locked. The robot arm is locked.

  • Green, Normal. The robot arm is on and ready for normal operation.

  • Red, Error. The robot is in a fault state, such as e-stop.

  • Blue, Transition. The robot is changing state, such as brake releasing.

Play

Starts the current loaded program.

Step

Allows a program to be run single-stepped.

Stop

Halts the current loaded program.

Speed slider

Manages the robot state. When RED, press it to make the robot operational.

Main Screen Icons

Icon Title Description
Move up

To move up a command node in a program tree.

Move down

To move down a command node in a program tree.

Revert

To revert a recent move of a command node in a program tree.

Undo revert

To undo revert a recent move of a command node in a program tree.

Suppress/Unsuppress

To suppress and unsuppress a command node in a program tree.

Copy

To copy a command node to another program tree.

Paste

To paste a command node to another program tree.

Cut

To cut a command node from a program tree.

Delete

To delete a command node in a program tree.