Icons

Left Header Icons

Icon Title Description

Operator

A simple means of operating the robot using pre-written programs.

Application

To configure the robot arm settings and external equipment, eg mounting and TCPs.

Program

Modifies the current robot program.

3D

Controls and/or regulates robot movement.

More

Access to About information and Settings.

About

Displays information about the robot.

Settings

To configure settings about the software, eg language and units.

Power

To power on or off the robot.

Safety Checksum

Displays the active safety checksum and detailed parameters, and change the operation mode.

Footer Buttons

Icon Title Description

Initialize

Manages the robot state. When RED, press it to make the robot operational.

  • Black, Power off. The robot arm is in a stopped state.

  • Orange, Idle. The robot arm is on, but not ready for normal operation.

  • Orange, Locked. The robot arm is locked.

  • Green, Normal. The robot arm is on and ready for normal operation.

  • Red, Error. The robot is in a fault state, such as e-stop.

  • Blue, Transition. The robot is changing state, such as brake releasing.

Play

Starts the current loaded program.

Step

Allows a program to be run single-stepped.

Stop

Halts the current loaded program.

Speed slider

Manages the robot state. When RED, press it to make the robot operational.