Password - Safety

Default Password

The default password for safety: ursafe

If you forget your password, it cannot be replaced or recovered.

You will have to reinstall the software.

You have to use the default password, when you change the password for the first time.

Change Safety Password

This is how you change the safety password in the PolyScope X settings.

  1. Click the hamburger menu in the top left corner.

  2. Click Settings.

  3. Click Safety in the Password section.

  4. Add the default password, if it is the first time.

  5. Add your preferred password, at least 8 characters.