Camera Cable
Description |
Your robot should be mounted and powered off before attaching the external cable and end effector. External cables can create risks of entanglement for the operator or interfere with robot operation. Cables can be damaged by the robot motion and create additional hazards. Care must be taken when affixing external cables that these risks are mitigated.
|
To affix the camera cable |
While robot joints can rotate plus and minus 360 degrees from the zero position, this movement will damage the camera cable and in practice is not required in most applications.
The safety functions of the robot can be used to limit the motions range of the joint. Refer to the robot User Manual for descriptions of how to use the safety functions.
|
Restricting joint movement |
When the camera cable is attached to the robot, you can restrict joint movement. Before continuing you should familiarize yourself with robot Freedrive, refer to the robot User Manual.
To restrict joints movement:
Read robot User Manual, Safety section on how to enter joint restrictions in PolyScope X.
|
Testing joint limits |
Try to move robot using the Move tab and verify that camera cable is not overtightened or clamped by possible robot movements.
|