Installing the software
Description |
The compute module of the AI Accelerator comes with pre-installed OS. Additional software, specific to AI Accelerator installed as Docker container on top of the Compute module's host OS. |
Installing the software |
During installation and configuration the Compute module should remain connected to the internet. Installation and configuration of the software components of AI Accelerator should be performed in the following order:
Each step is described in more detail below. |
To start the Compute module |
Remember to change the password at first boot. Leaving the password unchanged will expose the compute module to significant cybersecurity risks. |
To get software update |
|
To configure installation parameters |
|
To configure the robot |
|
To verify installation |
|
Troubleshooting |
If no camera view appears in URCaps running on the robot, check that ./scripts/run_ark.sh is running on Compute module.
|