Safely Setting the Active Payload
Before using Polyscope X, verify that the Robot Arm and Control Box are correctly installed.
-
On the Teach Pendant, press the emergency stop button.
-
On the Teach Pendant, press the power button and allow the system to start, loading Polyscope X.
-
Tap the Robot State Off button on the bottom left
-
Unlock the emergency stop button to change robot state from Emergency Stopped to Power off.
-
Step outside the reach (workspace) of the robot.
-
On the Initialize popup, tap the START button and allow robot state to change to Locked.
-
In the Payload field, in Active Payload, verify the payload mass. You can also verify the mounting position is correct, in the Robot graphic.
-
Tap the UNLOCK button, for the robot to release its brake system. The robot vibrates and makes clicking sounds indicating it is ready to be programmed