You access and activate different modes using Teach Pendant or the Dashboard Server.
If an external mode selector is integrated, it control the modes - not PolyScope or the Dashboard Server.
Automatic Mode When this mode is activated the robot can only execute a program of pre-defined tasks. You cannot modify or save programs and installations.
Manual Mode When this mode is activated you can program the robot. You can modify and save programs and installations.
The speeds used in Manual Mode must be limited to prevent injury. When the robot is operating in Manual Mode, a person could be positioned within reach of the robot.
The speed must be limited to the value that is appropriate for the application risk assessment.
Injury can occur if the speed used, while the robot is operating in Manual Mode, is too high.
Recovery Mode This mode activates when a safety limit from the active limit set is violated, the robot arm performs a Stop Category 0. If an active safety limit, such as a joint position limit or a safety boundary, is violated already when the robot arm is powered on, it starts up in Recovery mode. This makes it possible to move the robot arm back within the safety limits. In Recovery mode, the movement of the robot arm is restricted by a fixed limit that you cannot customize.
The robot performs a Safeguard Stop in Manual mode, if a Three-Position Enabling Device is configured, and either released (not pressed) or it is fully compressed.
Switching between Automatic mode to Manual mode requires the Three-Position Enabling Device to be fully released and pressed again to allow the robot to move.
|