Profinet
| Description |
The PROFINET network protocol enables or disables the connection of the robot to an industrial PROFINET IO-Controller. If the connection is enabled, you can select the action that occurs when a program loses PROFINET IO-Controller connection.
|
| Enable Profinet |
This is how you enable to Profinet function in PolyScope X.
|
| Using Profinet |
Find the profinet functions in PolyScope X:
In the PolyScope X left header.
Select the relevant action from the list:
|