Secure Shell (SSH) Access
Description |
You can manage remote access to the robot using Secure shell (SSH). The Secure shell security settings screen allows administrators to enable or disable SSH access to the robot.
|
To enable/disable SSH |
To the far right of the Enable SSH Access toggle button, the screen shows the port used for SSH communication. |
SSH Authentication |
Authentication can occur with a password and/or with a pre-shared, authorized key. Security keys can be added by tapping the Add Key button and selecting a security key file. Available keys are listed together. Use the trash icon to remove a selected key from the list. |