stopl(a, aRot=’a’)
Stop (linear in tool space)
Decelerate tool speed to zero
Parameters
a:
tool accleration [m/s^2]
aRot:
tool acceleration [rad/s^2] (optional), if not defined a, position acceleration, is used
Example command: stopl(20)
- Example Parameters:
- a = 20 m/s^2 -> rate of deceleration of the tool
- aRot -> tool deceleration [rad/s^2] (optional), if not defined, position acceleration, is used. i.e. it supersedes the "a" deceleration.