AprilTag
| Description |
AprilTags conceptually similar to QR codes, in that they encode data as two-dimensional grid of black and white squares. However, they differ in that the AprilTags not only carry data payload, but could be used for detecting tag position and orientation.
|
| Implementaton |
AI Accelerator software by default configured to use the 36h11 tag family in 30 mm size. Printable tags for the 36h11 family can be found at https://docs.cbteeple.com/robot/april-tags
Tag size can be configured in ros/launch/ark_pipeline_full.py
|
| Demo |
Tag recognition could be tested by opening the ark_example_tags. Switch to tags view in Dashboard URCap and observe the camera view updating at intervals. Tags can be configured for continuous detection by passing apriltags_continuous:=true as an argument to ark_pipeline_full in ros/scripts/run_ark.sh |
| The code for generating new families and instructions for using it can be found on github: https://github.com/AprilRobotics/apriltag-generation |