Camera
| Description |
The main options for camera mounting in the robot machine vision application are: robot-mounted or fixed-mounted. The camera mount included in AI Accelerator allows camera to be mounted on Universal Robots robot arms.
|
| Camera mount |
The AI Accelerator camera mount is designed to be inserted between the robot tool output flange and the end effector. Before mounting the camera, familiarize yourself with the Securing Tool section of the Mechanical Interface chapter in the robot User Manual and mounting instructions that came with the selected end effector.
|
| Assembly |
The camera mount is supplied pre-assembled. To attach camera to the mount:
|
| Camera cable |
Chapter Camera cable explains how to arrange the cable connecting the camera to compute module, externally along the robot arm.
|