Operational Mode
| Description |
Operational Modes are enabled in the UI, and protected by a password. They can additionally be configured by defining an Operational Mode Configurable I/O.
|
| Automatic Mode |
Once activated, the robot can only perform the loaded pre-defined task. The Application Tab, Program Tab, 3D Tab and Freedrive Mode are unavailable. You cannot load, modify, or save programs.
|
| Manual Mode |
Once activated, you can program the robot using the 3D and Move Tab, Freedrive Mode and Speed Slider. You can modify and save programs.
*** When tool power is enabled, a 400 ms soft start time begins allowing a capacitive load of 8000 uF to be connected to the tool power supply at start-up. Hot-plugging the capacitive load is not allowed. |
| Using Operational Mode Safety Input |
Using Operational Mode Safety Input
|
| Switching Modes |
To switch between modes, in the Right Header, select the profile icon to display the Mode Section.
PolyScope X is automatically in Manual Mode when the Safety I/O configuration with Three-Position Enabling Device is enabled.
|