Mounting Description

Description
Robot arm (Base) The robot arm uses six 8.8 strength, M10 bolts that fit into six 10.5 mm mounting holes in the base. The bolts shall be tightened to a torque of 45 Nm
Tool (Tool Flange) The tool uses six 8.8 strength, M8 bolts that fit into six M8 thread holes in the tool flange. The bolts shall be tightened to a maximum torque of 16 Nm.
Control Box The Control Box is wall mounted or placed on the ground.
Teach Pendant The Teach Pendant is wall mounted or placed onto the Control Box. Verify the cable does not cause tripping hazard. You can buy extra brackets for mounting the Control Box and Teach Pendant.

 

Warning:

IP rating

Mounting and operating the robot in environments exceeding the recommended IP rating can result in injury.

  • Mount the robot in an environment suited to the IP rating. The robot must not be operated in environments that exceed those corresponding to the IP ratings of the robot (IP54), Teach Pendant (IP54) and Control Box (IP44)

Warning:

Mounting
Unstable mounting can lead to accidents.
  • Always make sure the robot parts are properly and securely mounted and bolted in place.