Tool Analogue Inputs
| Description |
Tool Analogue Input are non-differential and can be set to either voltage (0-10V) or current (4-20mA) on the I/O tab. The electrical specifications are shown below.
Two examples of using Analog Input are shown in the following subsections. |
| Caution |
Analog Inputs are not protected against over voltage in current mode. Exceeding the limit in the electrical specification can cause permanent damage to the input. |
|
Using Tool Analog Inputs, Non-differential |
This example shows an analog sensor connection with a non-differential output. The sensor output can be either current or voltage, as long as the input mode of that Analog Input is set to the same on the I/O tab.
|
|
Using Tool Analog Inputs, differential |
This example shows an analog sensor connection with a differential output. Connecting the negative output part to GND (0V), works in the same way as a non-differential sensor.
|