`final
Three Position Enabling Device
| Description |
The robot arm is equipped with an enabling device in the form of the 3PE Teach Pendant. The Control Box supports the following enabling device configurations:
The illustration below shows how to connect a Three-Position Enabling device.
Note: The two input channels for the Three-Position Enabling Device input have a disagreement tolerance of 1 second. The UR robot safety system does not support multiple external Three-Position Enabling Devices.
|
| Operational Mode Switch |
Using a Three-Position Enabling device requires the use of an Operational Mode switch.
The illustration below shows an Operational Mode switch.
|