Controller I/O
| Common specifications for all digital I/O |
This section defines electrical specifications for the following 24V digital I/O of the Control Box. The word configurable is used for I/O configured as either safety-related I/O or normal I/O. These are the yellow terminals with black text.
Install the robot according to the electrical specifications which are the same for all three inputs. It is possible to power the digital I/O from an internal 24V power supply or from an external power source by configuring the terminal block called Power. This block consists of four terminals. The upper two (PWR and GND) are 24V and ground from the internal 24V supply. The lower two terminals (24V and 0V) in the block are the 24V input to supply the I/O. The default configuration uses the internal power supply (see below).
|
| Power supply |
If more current is needed, connect an external power supply as shown below.
The electrical specifications for both the internal and external power supply are shown below.
*3.5A for 500ms or 33% duty cycle.
|
| Digital I/Os |
The digital I/O are constructed in compliance with IEC 61131-2. The electrical specifications are shown below.
*For resistive loads or inductive loads of maximum 1H.
|