|
The Mini Displayport supports monitors using Displayport. This requires an active Mini Display to DVI or HDMI converter.
Passive converters do not work with DVI/HDMI ports.
The Fuse must be a UL marked, Mini Blade type with maximum current rating: 10A and minimum voltage rating: 32V
Connecting or disconnecting a Teach Pendant while the Control Box is powered on can cause damage.
Do not connect or disconnect the Teach Pendant while Control Box is powered on. This can cause damage to Control Box.
Failure to plug in the active adapter before powering on the Control Box can hinder the display output.
-
Plug in the active adapter before powering on the Control Box.
-
In some cases the external monitor must be powered on before the Control Box.
-
Use an active adapter that supports revision 1.2 as not all adapters function out-of-the-box.
|