pose_trans(p_from, p_from_to)
Pose transformation
The first argument, p_from, is used to transform the second argument, p_from_to, and the result is then returned. This means that the result is the resulting pose, when starting at the coordinate system of p_from, and then in that coordinate system moving p_from_to.
This function can be seen in two different views. Either the function transforms, that is translates and rotates, p_from_to by the parameters of p_from. Or the function is used to get the resulting pose, when first making a move of p_from and then from there, a move of p_from_to.
If the poses were regarded as transformation matrices, it would look like:
T_world->to = T_world->from * T_from->to T_x->to = T_x->from * T_from->to
Parameters
p_from: starting pose (spatial vector)
p_from_to: pose change relative to starting pose (spatial vector)
Return Value
resulting pose (spatial vector)
Example command: pose_trans(p[.2,.5,.1,1.57,0,0], p[.2,.5,.6,1.57,0,0])
- Example Parameters:
- p_1 = p[.2,.5,.1,1.57,0,0] → The first point
- p_2 = p[.2,.5,.6,1.57,0,0] → The second point
- Returns p[0.4,-0.0996,0.60048,3.14,0.0,0.0]