Clone Robot

Description

Use Backup Robot to create an image of the robot's internal storage on the data partition of the UR Disk Utility USB. You can use this image to restore the robot to the saved state.

Make sure that the UR Disk Utility USB has enough free space for the backup. Do not remove the UR Disk Utility USB drive while the backup is in progress.

Rules for naming the file:

  • A backup name can be up to 64 characters long.

  • A name can contain any characters, not only the letters A-Z and the numbers 0-9. Letters from other alphabets are also allowed.

  • Special characters are allowed, including but not limited to - . + ? ! @.

  • A slash (/) or a backslash (\) is not allowed anywhere in the name.

  • A space is allowed in the middle of a name.

Backup Robot Screen

 

Backup Robot
  1. On the main screen, select Backup Robot.

  2. In the Filename field, enter a name for the backup image.

  3. Select Backup.

  4. If a backup image with the same file name already exists, confirm that you want to overwrite it.

  5. Wait until the backup is complete. You cannot cancel the operation after it starts.

  6. When the operation is complete, return to the main screen.

Before the backup starts, select Cancel to return to the main screen without creating a backup.

A robot backup is for backup and recovery. Do not use Backup Robot to manage software across a fleet of robots.