| |
| Warnings
|
Conducting installation and/or maintenance of equipment connected to a power source can result in injury or death due to electric shock.
Incorrect mating or unmating can damage the Harting connector.
-
Do not twist the connector before it is fully seated.
-
Do not pull on the cable to disconnect the connector.
-
Do not rock or tilt the connector during mating or unmating.
Improper cable selection, usage, or connections can result in loss of power to the robot arm.
Connecting the Base Flange cable directly to any Control Box can result in damage to equipment and property.
Use the same mating and unmating steps at the Control Box connector and at the robot Base Flange connector. For the mating and unmating procedure, see Robot Cables (g-Series).
|
|
|
|
|